We recommend you download the My Ecodial S quick tour which clearly explains My Ecodial S in detail. You can download the My Ecodial S Quick Tour by clicking here.
You can download the My Ecodial S software for free by clicking here.
MyEcodial S calculates a branch of a low-voltage electrical installation, made up of an incomer, a distribution circuit and a load. Practically speaking, each level includes other outgoing circuits that must be taken into account when sizing the protective upstream devices. That is why there are equivalent loads which represent all the other outgoing circuits that are not presented in detail in the project.
Before displaying MV curve, the device has to be defined. First, go to the “Detailed properties” tab, then click on Q0 on the single diagram and finally fill in the properties form on the right. At this time, in front of “Definition mode”, choose “detailed” and follow the questionnaire.
My Ecodial S only manages 1 branche, if you need more, you should use My Ecodial L.
It is possible. Choose as type of project Extension to an installation in the Project tab, then continue to define the existing installation in the Network tab.