The best way to get My Ecodial L is to get in contact with your local Schneider-Electric sales agency.
My Ecodial doesn't build in UPS systems.
Up to 4 transformers can be parallel-connected.
Before starting My Ecodial L 3.4: go to "Start" / All programs / Schneider Electric/My Ecodial L 3.4/ languages choice - then click on the right language and start My Ecodial L 3.4.
Click on the bus bar, its becomes blue and dotted line, then click on the icon "Resize X and Y for the selection" (2 arrows and a black square under menus), two black squares appear at each end of the bus bars; pull on it to size the bar to the scale you would like.
This difference is due to the fact that the nominal current of the transformer is calculated by using the voltage at no-load and the nominal current of the generator is calculated by using the rated voltage. The use of the voltage at no-load is proved by the IEC 60076-1 standard.
Click on Menu Parameters / Diagram / Sheet model then click on the Number of sheets zone.
This can be done by exporting your diagram into a .dxf file. Do this by selecting from the menu: File > Print/Export. Then in the Print/Export window click on "Export" folder. Then save as a DXF file.